Technical FAQs

Ask a Question

"Error in GetSamples: Exception of type andapos;System.OutOfMemoryExceptionandapos; was thrown" when runing a Advanced Report in Crystal

Goals and Symptoms

Symptoms
Customer tries to run a report from Advanced Reports and sees the following error:

Error in GetSamples: Exception of type 'System.OutOfMemoryException' was thrown.

Causes and Fixes

Resolution

Restart all Crystal Services from Start/All Programs/ Crystal Enterprise 10/ Crystal Configuration Manager


Legacy KB System (APS) Data: RESL208988 V1.0, Originally authored by MaTh on 08/31/2012, Last Edited by MaTh on 08/31/2012
Related ranges: System Manager 4.2, System Manager 4.3
Was this helpful?
What can we do to improve the information ?