Technical FAQs

Ask a Question

ION OPC Data Access Server Service not in Services list

Goals and Symptoms

Summary
A customer's OPC client will not connect to the ION server to export data. When checking the Windows Services list to be sure the OPC Service is started and running, or to perform a service restart, the ION OPC Data Access Server service is no longer in the list.

Checking the setuplog file shows an error similar to:

OK (0) 6/13/2012 3:58:40 PM ERROR Unable to stop service PMLOPC. Time out exceeded. Could not stop ION OPC Data Access Server within 60 milliseconds 
OK (0) 6/13/2012 3:58:40 PM Removing service:PMLOPC

Causes and Fixes

Resolution

The service can be registered manually:

Open a command prompt, and type 'ION.OpcDaServer.exe -Service' and the service will re-appear in the services list.


Legacy KB System (APS) Data: RESL208811 V1.0, Originally authored by MaTh on 08/08/2012, Last Edited by MaTh on 08/08/2012
Related ranges: ION Enterprise V6.0
Was this helpful?
What can we do to improve the information ?