Technical FAQs

Ask a Question

Unable to generate a Power Load Profile report for ION devices in Web Reporter

The power load profile report looks for specific values that are not present in ION meters. The power load profile report may only be ran on Powerlogic devices.


Legacy KB System (APS) Data: RESL208809 V1.0, Originally authored by MaTh on 08/07/2012, Last Edited by MaTh on 08/07/2012
Related ranges: Power Monitoring 7.0, ION Enterprise V6.0
Was this helpful?
What can we do to improve the information ?