Technical FAQs

Ask a Question

Does the Model 98 have to be run in 4 wire mode?

The Model 98 can be run in 2 wire rs485 mode by jumpering the plus and minus terminals.
As with any modbus daisy chain, do not switch between 2-wire and 4-wire comms without an adapter such as the CNV100.


Legacy KB System (APS) Data: RESL208787 V1.0, Originally authored by MaTh on 08/04/2012, Last Edited by MaTh on 08/04/2012
Related ranges: Model 98 DTC
Was this helpful?
What can we do to improve the information ?