Technical FAQs

Ask a Question

EGX300 custom webpage to allow register writes to devices

The attached file is a custom webpage for the EGX300 that will enable the gateway to write to registers. This page needs to be transferred to the EGX FTP webpage under the Monitoring folder.
1. Launch Windows Explorer, type ftp:// and the IP address of the EGX (for example, ftp://169.254.0.10) in the Address text box, then press Enter.
2. Type the user name Administratorand the administrator password in the text boxes, then click Log On.
3. Open a new Windows Explorer window, locate the custom web page you want to send to the EGX, right-click it, then click Copy.
4. Switch back to the EGX Windows Explorer window you opened in Step 1, then open the folder where the web page will be copied (/www/monitoring/).
5. Right-click in the right pane of the Windows Explorer window, then click Paste. NOTE: Instead of copying and pasting the file, you can drag-and-drop the file into Windows Explorer.
6. Click Close on the Windows Explorer window.

write.htm


Legacy KB System (APS) Data: RESL208659 V1.0, Originally authored by MaTh on 07/17/2012, Last Edited by MaTh on 07/17/2012
Related ranges: EGX300
Was this helpful?
What can we do to improve the information ?