Technical FAQs

Ask a Question

Why is the date always 1/1/1971 for a Power-up/Reset on a Micrologic Trip Unit?

The reason the date shows 1/1/1971 for a Power-up/Reset is because the time and date are stored in volatile memory which gets reset to default after a loss in control power. Once a time sync is ran on the Trip Unit the correct time and date will be displayed.


Legacy KB System (APS) Data: RESL208588 V1.0, Originally authored by MaTh on 07/06/2012, Last Edited by MaTh on 07/06/2012
Related ranges: Micrologic
Was this helpful?
What can we do to improve the information ?