Technical FAQs

Ask a Question

Why is the Front Panel password limited to 4 digits when using the Advanced Options Security Wizard in ION Setup 3.0?

Using security wizard in ION Setup 3.0, the front panel password (meter password, standard security password) is limited to four digits while front panel password can actually be up to eight digits. This means, using the wizard, the new front panel password can not be set to a number with more than four digits.
The work around is to use Advanced Mode to change / setup security on the meter instead of using the wizard.

This problem will be corrected in the next release of ION Setup.


Legacy KB System (APS) Data: RESL208565 V1.0, Originally authored by MaTh on 07/02/2012, Last Edited by MaTh on 07/02/2012
Related ranges: ION Setup 2.2
Was this helpful?
What can we do to improve the information ?