Technical FAQs

Ask a Question

What devices are natively supported in ION Enterprise (IONE) 5.6 SP2?

ION 5.6 SP2 Supported Device Types:
PM800
PM700
PM200
Micrologic P
Micrologic H
Micrologic E Compact NSX
Micrologic A Compact NSX
Micrologic A
ION 8800
ION 8600
ION 8500
ION 8400
ION 8300
ION 7700
ION 7650
ION 7600
ION 7550 RTU
ION 7550
ION 7500
ION 7500 RTU
ION 7350
ION 7330
ION 7300
ION 6200 (Modbus)
ION 6200
CM4000
CM3000
BCPM
ACCESS 9700
ACCESS 9610
ACCESS 9600
ACCESS 9510 RTU
ACCESS 9510
ACCESS 9500 RTU
ACCESS 9500
ACCESS 9350
ACCESS 9330
ACCESS 9300
ACCESS 9200 (MODBUS)
ACCESS 9200
3800 RTU
3720 ACM
3710 ACM
3300 ACM


Legacy KB System (APS) Data: RESL208564 V1.0, Originally authored by MaTh on 07/02/2012, Last Edited by MaTh on 07/02/2012
Related ranges: ION Enterprise V5.6
Was this helpful?
What can we do to improve the information ?