Technical FAQs

Ask a Question

RS2008 Configuration Wizard cannot connect to Reporting Services with COM Exception (0x80040208)

The RS2008ConfigurationWizard can give the error (0x80040208) under the following circumstances:
1. The SQL Reporting Services (<Instance Name>) service is not running.
2. The RS2008WRConfigWizard needs to be run as an Administrator (Right click-> "Run as administrator")


Legacy KB System (APS) Data: RESL208502 V1.0, Originally authored by MaTh on 06/26/2012, Last Edited by MaTh on 06/26/2012
Related ranges: Power Monitoring 7.0, ION Enterprise V6.0
Was this helpful?
What can we do to improve the information ?