Technical FAQs

Ask a Question

Can the digital inputs (pulse inputs) of the PowerLogic E4800 (EM4800) be replaced without replacing the whole meter?

The pulse inputs cannot be individually replaced because they are integrated into the circuit board. The entire meter will need to be returned for repair.


Legacy KB System (APS) Data: RESL208492 V1.0, Originally authored by MaTh on 06/23/2012, Last Edited by MaTh on 06/23/2012
Related ranges: EM4800
Was this helpful?
What can we do to improve the information ?