Technical FAQs

Ask a Question

What do the letters A, B, C and D designate when looking at ION Modules?

The letters A, B, C and D after a module name refer to the TOU (Time of Use) season.  

For example:
kW sd mx A


Legacy KB System (APS) Data: RESL208485 V1.0, Originally authored by MaTh on 06/22/2012, Last Edited by MaTh on 06/22/2012
Related ranges: ION Other, ION Setup 2.2, Power Monitoring 7.0, ION Enterprise V6.0, ION Enterprise V5.6
Was this helpful?
What can we do to improve the information ?