Technical FAQs

Ask a Question

What is the life expectancy of a PowerLogic E4800?

The life expectancy of the E4800 (EM4800) is from 10 to 15 years. The document below can be sent to the customer if documentation is needed.
EM4800 Expected Life.pdf


Legacy KB System (APS) Data: RESL207837 V1.0, Originally authored by MaTh on 04/04/2012, Last Edited by MaTh on 04/04/2012
Related ranges: EM4800
Was this helpful?
What can we do to improve the information ?