Technical FAQs

Ask a Question

SPM 7.0 - After upgrading from ION Enterprise 6.0, when I run a saved report, no measurements are selected.

During the database upgrade required for SPM 7.0, a number of measurements were remapped to different IDs. If a report configured and saved prior to the upgrade from ION Enterprise 6.0 to Power Monitoring 7.0 referenced measurements that were remapped, the saved reports will lose their links to the selected measurements, resulting in the behaviour described. To correct this, it is necessary to re-select the desired measurements, i.e. reconfigure the report, and then re-save it.
This is most likely to happen with 100 ms reports using CM4000 data, and WAGES data.

Last Revised: March 19, 2012

Internal

All content © 1992-2012 Schneider Electric

 


Legacy KB System (APS) Data: RESL207712 V2.0, Originally authored by JaMc on 03/20/2012, Last Edited by JaMc on 05/17/2012
Related ranges: Power Monitoring 7.0
Was this helpful?
What can we do to improve the information ?