Technical FAQs

Ask a Question

Text is displayed incorrectly in Event Notfication Solution (ENS) 6.4 (Text is all capitalized)

Goals and Symptoms

Symptoms
All the text on ENS 6.4 pages is capitalized and sometimes rendered incorrectly.



Facts and Changes

Key Words

Capital letters, lined up incorrectly, missing spaces

Causes and Fixes

Cause

Installation is missing the resources.dll file


Resolutions

1) Browse to the location where ENS is installed.
2) Navigate to the folder called "Common" inside the "Event Notification Solution" directory.
3) Paste the attached resources.dll file into this directory.
4) Restart IIS.
5) Now all web pages should render text correctly.

Attachments

(Removed File URL: 207465_220E/Resources.dll)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/5a25c37319d90c19c12579ac001612dc/fl_block_5/0.E2?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL207465 V1.0, Originally authored by MaTh on 02/22/2012, Last Edited by MaTh on 02/22/2012
Related ranges: SMS Add-on, Paging Module
Was this helpful?
What can we do to improve the information ?