Technical FAQs

Ask a Question

Incorrect description of energy objects unit of measure within the SchneiderPm8EccV01_00.mib file

Goals and Symptoms

Symptoms


  • The description strings of the energy objects contained in the MIB are incorrect. The descriptions indicate the objects are reported in kilowatt-hours when they are actually reported in watt-hours.

    The objects affected include:
    · eReal Energy (.1.3.6.1.4.1.3833.1.7.255.15.1.1.9.1.2)
    · eReactiveEnergy (.1.3.6.1.4.1.3833.1.7.255.15.1.1.9.1.4)
    · eApparentEnergy (.1.3.6.1.4.1.3833.1.7.255.15.1.1.9.1.6)

    These energy objects are correctly reported in watt-hours, only the description is incorrect.

Facts and Changes

Customers Effected: Customers effected by this issue is limited to the ones using SNMP protocol to collect energy data from the PM800 series Power Meters.

Causes and Fixes

Solution

Replace the MIB file SchneiderPm8EccV01_00.mib with SchneiderPm8EccV01_10.mib

SchneiderPm8eccV01_10.mib


Legacy KB System (APS) Data: RESL207375 V1.0, Originally authored by MaTh on 02/11/2012, Last Edited by MaTh on 02/11/2012
Related ranges: PM8ECC, PM800 series
Was this helpful?
What can we do to improve the information ?