Technical FAQs

Ask a Question

What TCP Port do ION Meters use for DNP v3.0 via Ethernet?

Issue:
A user needs to know what TCP port is used for the DNP 3.0 protocol when connecting to a meter via Ethernet.

Product Line:
ION meters

Environment:
ION meters

Cause:
A user may not have documentation stating this information.

Resolution:
TCP port 20000 is used for the DNP v3.0 protocol via the Ethernet port.
Was this helpful?
What can we do to improve the information ?