Technical FAQs

Ask a Question

Can the ION7700 time synchronize downstream devices?

The ION7700 is not capable of time synching downstream devices by itself. The user will need to use software such as ION Setup or ION Enterprise to create time synch packets. The meter will; however, relay time synch packets to downstream devices if configured as an Ethergate connection.


Legacy KB System (APS) Data: RESL207166 V1.0, Originally authored by MaTh on 01/17/2012, Last Edited by MaTh on 01/17/2012
Related ranges: ION Other
Was this helpful?
What can we do to improve the information ?