Technical FAQs

Ask a Question

Is there a workaround for the 'Chain of links too long - Max 8' error in ION Enterprise or ION Setup?

This is a normal limitation of the software.
Possible resolution
Reduce the number of modules in the chain of links to less than 8.

Possible work-around
Include a feedback module in the chain of links.


Legacy KB System (APS) Data: RESL207083 V1.0, Originally authored by MaTh on 01/09/2012, Last Edited by MaTh on 01/09/2012
Related ranges: ION Setup 2.2, ION Enterprise V6.0, ION Enterprise V5.6
Was this helpful?
What can we do to improve the information ?