Technical FAQs

Ask a Question

Do ION Meters support string tags for SNMP identifiers?

Some Powerlogic meters like PM800, allow the user to assign a string as a name identifier for SNMP. However, the SNMP modules in ION Meters only support numeric inputs. The only option would be to attach unique numeric data to one of the SNMP inputs and use that.


Legacy KB System (APS) Data: RESL206998 V1.0, Originally authored by MaTh on 12/28/2011, Last Edited by MaTh on 12/28/2011
Related ranges: ION8600, ION7550/ION7650, ION7550 RTU
Was this helpful?
What can we do to improve the information ?