Technical FAQs

Ask a Question

How do the Severity Levels in Active Pager Module (APM) correspond to alarm levels in System Management Software (SMS)?


Below is a table of how Severity(APM) corresponds to SMS alarm and Meter onboard alarm level.

APM SMS Onboard Alarm Level
1000 Comms Loss
900 1 1
800 2 2
700 3 3
600 4
500 5
400 6
300 7
200 8
100 9

Please note it's always best practice to have the severity +/-1 of the severity level.

For Example: If the customer wants only Level 4 Alarms, a filter would be created with severity from 599 to 601.


Legacy KB System (APS) Data: RESL206964 V1.0, Originally authored by MaTh on 12/22/2011, Last Edited by MaTh on 12/22/2011
Related ranges: SMS Add-on, Paging Module
Was this helpful?
What can we do to improve the information ?