Technical FAQs

Ask a Question

Is Event Notification Solution 6.4 /Active Pager Module 6.4 (ENS 6.4, APM 6.4) compatible with SQL 2000?

ENS 6.4 is only supported with SQL 2005 and SQL 2008 instances.
During the install, SQL 2000 instances can be chosen, but the install will not complete if a SQL 2000 instance is selected.


Legacy KB System (APS) Data: RESL206608 V1.0, Originally authored by MaTh on 11/09/2011, Last Edited by MaTh on 11/09/2011
Related ranges: Paging Module, SMS Add-on
Was this helpful?
What can we do to improve the information ?