Technical FAQs

Ask a Question

How many stop bits does the EGX support?

Issue
How many stop bits does the EGX support?

Product Line
EGX100, EGX200, EGX300, EGX400

Cause
Customer would like to know number of stop bits supported by EGX gateway. 

Resolution
All EGX devices use an 11-bit frame serial frame. 1 start-bit, 8 data-bits, and 1 or 2 stop bits depending on the parity selection.

The number of stop bits is taken according the parity settings shown below:
Even parity: 1 Start-Bit, 8 Data-Bits, 1 Parity-Bit, 1 Stop-Bit
Odd parity: 1 Start-Bit, 8 Data-Bits, 1 Parity-Bit, 1 Stop-Bit
No parity: 1 Start-Bit, 8 Data-Bits, 2 Stop-Bits

Was this helpful?
What can we do to improve the information ?