Technical FAQs

Ask a Question

What type of communications connector is used by the Circuit Monitor 2000 (CM2) Portable's 232 port?

The CM2 Portable meter comes utilizes a RS232 DB25 connector. The user will need a custom PCMCOMM232 cable. Please see the following PINOUT


Legacy KB System (APS) Data: RESL206468 V1.0, Originally authored by MaTh on 10/24/2011, Last Edited by MaTh on 10/24/2011
Related ranges: CM2000 series
Was this helpful?
What can we do to improve the information ?