Technical FAQs

Ask a Question

Is is possible for System Manager Software (SMS) Information Manager to automatically email reports

This is possible with some specific configuration. SMS allows the user to configure email tasks which can include a Information Manager (IM) report. When configuring the IM report, the user should select to 'save report' with a specific name. The user should also schedule the report to run 'automatically on a scheduled basis' and include the 'overwrite' option. Finally, the user can configure a scheduled task to email the report as an attachment. Select the .html file and .jpg (if necessary) as the attachments. The default report location is c:\powerlogic\infomanager\reports\. Although the email tasks is emailing the same file each time, by selecting the overwrite option the file will be updated with new data each time the report is run.

Was this helpful?
What can we do to improve the information ?