Technical FAQs

Ask a Question

Which side of the fiber connector is RX and which is TX for the ECC21 fiber optic port?

The connection that is nearest the ethernet port is RX, the connection closest to the RS-485 port is TX.


Legacy KB System (APS) Data: RESL206466 V1.0, Originally authored by MaTh on 10/24/2011, Last Edited by MaTh on 10/24/2011
Related ranges: ECC21
Was this helpful?
What can we do to improve the information ?