Technical FAQs

Ask a Question

Crystal Report Viewer Error: The crysal report viewer is unable to create it's resource objects

When attempting to view a generated report, the following error is displayed:
The crystal report viewer is unable to create it's resource objects



To resolve this error go to start > all programs > crystal enterprise 10 > crystal configuration manager
1. Restart the Crystal Management Server
2. Restart all other Crystal services EXCEPT Crystal Web Component Server
3. Restart Internet Explorer
4. View the report


Legacy KB System (APS) Data: RESL206225 V1.0, Originally authored by MaTh on 09/22/2011, Last Edited by MaTh on 09/22/2011
Related ranges: SMS Add-on
Was this helpful?
What can we do to improve the information ?