Technical FAQs

Ask a Question

What device types are compatible with PowerView 2.0.1?

Natively, PowerView supports the following device types:
Compact NSX A
Compact NSX E
Compact NSX E - Motor
Enercept Basic
Enercept Enhanced
ION6200
MC08
MC09
MC18
Micrologic A
Micrologic H
Micrologic P
PM210
PM500
PM710
PM750
PM820
PM850
PM870
PM9C


The following are optional device type installs:

CM2350
CM3000
CM4000
CampctNSX
PM600
SEPAM20
SEPAM40
TWIDO


Legacy KB System (APS) Data: RESL205974 V1.0, Originally authored by MaTh on 08/09/2011, Last Edited by MaTh on 08/09/2011
Related ranges: PowerView
Was this helpful?
What can we do to improve the information ?