Technical FAQs

Ask a Question

Is it possible to change the quantity scale factors in Micrologic Trip Units?

The Micrologic Trip Units have a particular scale factor associated with each quantity which cannot be changed. These scale factors can be found in the "Using MICROLOGIC® Electronic Trip Units in a
POWERLOGIC® System" manual 63220-080-200B1.


Legacy KB System (APS) Data: RESL205870 V1.0, Originally authored by MaTh on 07/27/2011, Last Edited by MaTh on 07/27/2011
Related ranges: Communication with Micrologic trip units
Was this helpful?
What can we do to improve the information ?