Technical FAQs

Ask a Question

Is it possible to monitor loads above 2400A with the Enercept Meter?

Veris Industries manufactures Multi-turn coils which make this application possible. Reference the below document which describes the process when using the Multi-turn coils.
vn19_CoilLoopsFor2400+Loads.pdf


Legacy KB System (APS) Data: RESL205867 V1.0, Originally authored by MaTh on 07/27/2011, Last Edited by MaTh on 07/27/2011
Related ranges: Enercept
Was this helpful?
What can we do to improve the information ?