Technical FAQs

Ask a Question

Unable to preview system reports in System Manager Software (SMS) Setup utility

A printer must be added to the computer to be able to preview the reports that are generated using system reports. Any printer will work, even if it is not connected to the machine.


Legacy KB System (APS) Data: RESL205866 V1.0, Originally authored by MaTh on 07/27/2011, Last Edited by MaTh on 07/27/2011
Related ranges: System Manager 4.3, System Manager 4.0, System Manager 4.2
Was this helpful?
What can we do to improve the information ?