Technical FAQs

Ask a Question

Branch Circuit Power Meter Split Core (BCPMSC) CTs are marked 60A

Goals and Symptoms

Summary
The BCPMSC CT options include 50A and 100A models

Facts and Changes

Information

The CTs provided by Veris are current transducers with a 0.333V output. The BCPMSC has been scaled to accommodate this. This is not intended for use on hardware applications requiring above 50A but below 100A. CTs shipped with the 50A model are specified to function within:

2% of Current reading from 2-100%
3% of Power reading from 2-100%

Causes and Fixes

Use the CTs that are provided.


Legacy KB System (APS) Data: RESL205855 V1.0, Originally authored by MaTh on 07/27/2011, Last Edited by MaTh on 07/27/2011
Related ranges: BCPM(Branch Circuit Power Meter)
Was this helpful?
What can we do to improve the information ?