Technical FAQs

Ask a Question

What are the excitation points and secondary ratings of the Brance Circuit Power Meter Split Core (BCPMSC) CTs?

CTs metering the mains are 0.333V secondary transducers.
CTs metering the branches are 800mA secondary transducers.
Excitation point of the mains CTs are 0.25A.
Excitation point of the branch Cts are 10% of the rated value.
CTs shipped with the meter are labeled as 60A Cts, however they are specified to function within 1% accuracy up to 50A.


Legacy KB System (APS) Data: RESL205846 V1.0, Originally authored by MaTh on 07/26/2011, Last Edited by MaTh on 07/26/2011
Related ranges: BCPM(Branch Circuit Power Meter)
Was this helpful?
What can we do to improve the information ?