Technical FAQs

Ask a Question

Can the E4800 and EM4800 push information to the root directory of an FTP site?

The E4800 and EM4800 Host Server configuration cannot be blank, but if a '\' is put in the Upload/Download directory, the meter interprets that as the root directory.
Below is an example of an FTP site (IP address 10.10.10.10) that receives the report files at the root directory.


Legacy KB System (APS) Data: RESL205834 V1.0, Originally authored by MaTh on 07/26/2011, Last Edited by MaTh on 07/26/2011
Related ranges: EM4800
Was this helpful?
What can we do to improve the information ?