Technical FAQs

Ask a Question

"Object Required" error message when opening the Events page in Sequence of Events Recorder 7.x (SER)

Goals and Symptoms

Symptoms
When accessing the Events page in SER 7.x using Internet Explorer 8 (IE8), the user receives the following pop-up error message:

Object Required

Causes and Fixes

Cause

When accessing SER 7.x using Internet Explorer 8, the page must be displayed in Compatibility Mode / Compatibility View


Resolution

Place IE8 into compatibility mode by either going to Tools->Compatibility View or clicking the compatibility view icon on the address bar.


Legacy KB System (APS) Data: RESL205639 V1.0, Originally authored by MaTh on 06/30/2011, Last Edited by MaTh on 06/30/2011
Related ranges: Sequence of Events Recorder (SER)
Was this helpful?
What can we do to improve the information ?