Technical FAQs

Ask a Question

PowerLogic E5600: Display Indicator Definitions

List of meanings for the E5600 Display Indicators:
R / C - Remote Communication: Appears on the meter display when an AMR device is communicating with the meter.
P / R - Programmer Reader: Appears on the meter display when optical communication is taking place.
Z / B - Zigbee: Appears on the meter display when a zigbee device is communicating with the meter.
OPN - Open: Appears on the meter display when the service disconnect switch is in the open state.
ARM - Appears on the meter display when the service disconnect switch is armed to be closed by either a network command or pushing the reconnect button on the cover.
CLS - Close: Appears on the meter display when the service disconnect switch is closed.
Z / F - Zero Fill: Appears on the meter display when the meter is in catch up and fills the load profile intervals with zeroes.
S / B - Stand By: Appears on the meter display when the meter is waiting for the date and time to be set either optically or by communication.
C / U - Catch Up: Appears on the meter display when the meter has exited stand by mode and is back filling time of use registers.


Legacy KB System (APS) Data: RESL205441 V1.0, Originally authored by MaTh on 06/01/2011, Last Edited by MaTh on 06/01/2011
Related ranges: E5600
Was this helpful?
What can we do to improve the information ?