Technical FAQs

Ask a Question

ION7700 Meter Template File


Standard Template - ION 7700 V210 : 7700_V210_FAC-4WYE_V1.1.1.exe

 
You can install meter templates using ION Setup or ION Enterprise. See the "Upgrading ION Device Firmware" technical note for complete details.

Install Templates with ION Setup

1. Download the device template and save it to your ION Setup TEMPLATE folder (select the file below that matches your meter's feature set).

Use these .DCF files with ION Setup to perform firmware upgrades. These are default meter templates only. If you have custom programming in your meter, create your own template file before performing the firmware upgrade.

2. Follow the upgrade procedures outlined in the "Upgrading ION Device Firmware" technical note.

Key Words and Phrases: .dcf, device configuration file, framework

Legacy KB System (APS) Data: RESL205245 V1.0, Originally authored by DaMi on 04/30/2011, Last Edited by DaMi on 04/30/2011
Related ranges: ION7700
Was this helpful?
What can we do to improve the information ?