Technical FAQs

Ask a Question

ION7700 Firmware V220

 

V220 - Released June 28, 2002


V220 : 7700 V220.exe

The ION 7700 consists of three distinct components; the meter, the Xpress card, and the MGT. Each component has its own firmware that must be upgraded.

NOTE: The ION 7700 must be upgraded in the following order:

(1) Xpress card, (IMPORTANT: older cards must be upgraded through com 2)

(2) Meter,

(3) MGT. If you upgrade in the wrong order, some modules will not restore properly.

Features

    • Enhanced Arithmetic Module capability
    • More robust Ethernet stack
    • Improved interface with the MGT module
 
Component Firmware Version
ION 7700 V220
Xpress Card V2164_XP
MGT V2011

Key Words and Phrases: 7700V220.upg, mgt2011.upg, XPR_V2164.upg

Legacy KB System (APS) Data: RESL205241 V1.0, Originally authored by DaMi on 04/30/2011, Last Edited by DaMi on 04/30/2011
Related ranges: ION7700
Was this helpful?
What can we do to improve the information ?