Technical FAQs

Ask a Question

ION7600 Firmware V254


V254 (Jan. 2008) - 1 Amp & 5 Amp (Class 2 - Class 20): 7600V254.exe


When upgrading your meter's firmware please download the latest firmware version (.upg file) and the equivalent Meter Template (.dcf file).

You can upgrade meter firmware using ION Setup or ION Enterprise. See the "Upgrading ION Device Firmware" technical note for complete details.


Legacy KB System (APS) Data: RESL205223 V1.0, Originally authored by DaMi on 04/30/2011, Last Edited by DaMi on 04/30/2011
Related ranges: ION7500/ION7600
Was this helpful?
What can we do to improve the information ?