Technical FAQs

Ask a Question

Is it possible to change the datalog record count in a PM800 (PM8)?

Issue
Can the record count in the data logs be changed for the PM800 series meters?

Product Line
PM800 series

Environment
Data Logs

Resolution
Because of the way the memory is addressed in the PM800 series meters, the record count is automatically determined based off the template assigned to the log. The record count can not be manually changed via SMS or register writes

 

Was this helpful?
What can we do to improve the information ?