Technical FAQs

Ask a Question

PowerLogic Device Support in ION Enterprise 5.6 Service Pack 1


See attached document:

PowerLogic_Device_Support_in_ION_Enterprise_5.6_Service_Pack_1.pdf

This technical note explains how to set up the PowerLogic® PM series devices, CM series devices and MicroLogic trip units, for use with ION Enterprise.

PUBLICATION NOTE: This document is published here under the FAQ document type because it is much easier and faster to make the document available on the appropriate powerlogic knowledgebase portals using the APS software tool than by using the strictly more appropriate (but generally more time-consuming) Schneider EDMS publication tool.


Legacy KB System (APS) Data: RESL205117 V1.0, Originally authored by ViWa on 04/16/2011, Last Edited by ViWa on 04/16/2011
Related ranges: ION Enterprise V5.6
Was this helpful?
What can we do to improve the information ?