Technical FAQs

Ask a Question

Why does the Enercept Meter instantaneous table displays average L-L voltage that is lower/higher than any of the individual L-L voltages?

The PowerLogic Enercept Meter calculates the average L-L voltage based off the previous sample's (1 second registers) L-L readings, therefore when displaying an instantaneous table, the user could see numbers for L-L voltages that are lower or higher than the average L-L voltage.


Legacy KB System (APS) Data: RESL205054 V1.0, Originally authored by MaTh on 04/12/2011, Last Edited by MaTh on 04/12/2011
Related ranges: Enercept
Was this helpful?
What can we do to improve the information ?