Technical FAQs

Ask a Question

Are the split core CTs from the Branch Current Monitor Split Core(BCMSC) and the Branch Circuit Power Meter Split Core(BCPMSC) interchangeable?

The CTs between the BCMSC and BCPMSC are interchangeable, but please note there are 50A and 100A CT variants.


Legacy KB System (APS) Data: RESL204838 V1.0, Originally authored by MaTh on 03/17/2011, Last Edited by MaTh on 03/17/2011
Related ranges: BCPM(Branch Circuit Power Meter), BCM (Branch Current Monitor)
Was this helpful?
What can we do to improve the information ?