Technical FAQs

Ask a Question

Is it possible to use the current sensor strip from one Branch Circuit Power Meter (BCPM) model (A/B/C) to another?

It is possible to interchange the CT strips, but the user will encounter the following issues:
1. Accuracy of the BCPM will drop to approximately 5% of reading.
2. The error LED will illuminate on the BCPM Circuit Board. The serial numbers of the circuit board and sensor strips are encoded together. If the BCPM senses that the serial numbers do not match, the error LED will illuminate.

It is recommended to use the current sensor strips that came with the unit and are therefore calibrated together.


Legacy KB System (APS) Data: RESL204837 V1.0, Originally authored by MaTh on 03/17/2011, Last Edited by MaTh on 03/17/2011
Related ranges: BCPM(Branch Circuit Power Meter)
Was this helpful?
What can we do to improve the information ?