Technical FAQs

Ask a Question

What are the EN50160 definitions?

The following document includes definitions included in the EN50160 standard.
The application of the EN50160 standard is included in the meter reference manuals (PM8's, CM4's, CM3's, etc).

DraftStandard0026rev2-DraftEN501602005-05.pdf


Legacy KB System (APS) Data: RESL204836 V1.0, Originally authored by MaTh on 03/17/2011, Last Edited by MaTh on 03/17/2011
Related ranges: Standards Applied to Power Management PRODUCTS
Was this helpful?
What can we do to improve the information ?