Technical FAQs

Ask a Question

For a Sub Meter Display (SMD, SMDOPN, SMD63, SMD63M, or SMD63M1), should the Address Routing be ON or OFF?

Issue
When should address routing be set to ON or OFF for a sub meter display?

Product Line
Sub Meter Display (SMD, SMDOPN, SMD63, SMD63M, or SMD63M1)

Environment
Address Routing

Resolution
Address Routing should be set to the following as per the application:
ON = upstream communication is disabled
OFF = upstream communication is enabled

This setting is under the "Setup Communications" menu (4th submenu).

Was this helpful?
What can we do to improve the information ?