Technical FAQs

Ask a Question

Why does the PowerLogic E5600 display "C/U" instead of "R/C"?

When the E5600 displays C/U on the front display, the meter is in the process of filling the Load Profile with zeros. Typically this would happen after a power outage or interruption.


Legacy KB System (APS) Data: RESL204743 V1.0, Originally authored by MaTh on 03/05/2011, Last Edited by MaTh on 03/05/2011
Related ranges: E5600
Was this helpful?
What can we do to improve the information ?