Technical FAQs

Ask a Question

Is it possible to change the scale factor for quantities in a Branch Circuit Power Meter (BCPM) or Branch Current Monitor (BCM)?

The BCM reports the values in mA and the BCPM auto-scales the values. For both meters, the scale factors are unchangeable.


Legacy KB System (APS) Data: RESL204741 V2.0, Originally authored by MaTh on 03/05/2011, Last Edited by MaTh on 03/14/2011
Related ranges: BCPM(Branch Circuit Power Meter), BCM (Branch Current Monitor)
Was this helpful?
What can we do to improve the information ?