Technical FAQs

Ask a Question

Point-to-Point Protocol (PPP) configuration for the PowerLogic EM4800

Which settings are relevant to Point-to-Point communication?

Product Line
EM4800 E4800

Configuration Tool

Point-to-Point Protocol or PPP is a encapsulation protocol for transporting IP traffic over dial-up point-to-point links, effectively allowing serial communications through a dial-up telephone connection.

The following settings apply to most situations:

Phone #: (required)
AT String: AT X3
Wait for Dial Tone: unchecked if there is a message waiting tone service enabled
PPP Login: (required)

Was this helpful?
What can we do to improve the information ?