Technical FAQs

Ask a Question

How is it possible to determine if an Enercept Meter is the Basic or Enhanced model?

A System ID register located at addresses 30 (Integer) and 315 (Float) exists within the Enercept Meter. Reading that register will yield one of two values:
A value of 15022 will be returned from the Enhanced Enercept model.
A value of 15023 will be returned from the Basic Enercept model.

Was this helpful?
What can we do to improve the information ?