Technical FAQs

Ask a Question

The Collect Procedure for the "DTSPipeline" service in DLL "C:\Program Files\Microsoft SQL Server\90\DTS\Binn\DTSPipelinePerf.dll" generated an exception or returned an invalid status

Goals and Symptoms

Symptoms
The following error message is displayed in the Windows Application Event Log:

The Collect Procedure for the "DTSPipeline" service in DLL "C:\Program Files\Microsoft SQL Server\90\DTS\Binn\DTSPipelinePerf.dll" generated an exception or returned an invalid status.

There will be one message from the source Perflib and one from MSSQL$POWERLOGIC

Causes and Fixes

Cause

This is a known issue in Microsoft SQL Server 2005 and Microsoft SQL 2005 Express. This is a information message only and does not affect the operation of the system.


Resolution

This error message has been corrected in SQL Server 2005 SP4 and SQL 2005 Express SP4.

To obtain SQL Server 2005 SP4, visit the following Microsoft Web site:
http://go.microsoft.com/fwlink/?LinkID=204632

To obtain SQL Server 2005 Express Edition SP4, visit the following Microsoft Web site:
http://go.microsoft.com/fwlink/?LinkID=204633

Was this helpful?
What can we do to improve the information ?